SYSTem:DCPS[:STATe]?

(Read-only) Query the present voltage source state.

NOTE: This command supersedes SYST:VVS? for D-series (Fluyt) models. To learn  more, refer to Replacement Commands topic.

Relevant Modes

ALL Modes.

ALL models with Option 309 (Voltage Source)

Parameters

N/A

Examples

N/A

Query Syntax

SYST:DCPS? */Query the present voltage source state

Return Type

string - Returns one of the following:

  • OFF - Voltage source disabled. OutputEnable is not selectable.

  • OUTPUTDISABLED - Voltage source enabled but OutputEnable is set to OFF.

  • INTRANSITION - When DCPS is switching between states. It should be pretty quick and most of the times not seen (in test code maybe a 2-3s wait time is more than enough to detect a latch up or error). 

  • READY - Voltage source enabled and OutputEnable automatically set to ON. 

  • TRIPPED - Current overload causing the fault line to trigger (output voltage should become 0V after tripped). To clear a 'TRIPPED' state, send SYSTem:DCPS:CLR. 

  • CURRENTLIMITED - Current limited causing voltage dropout (output voltage is a at least 200mV lower than set voltage in current limited condition). To clear a 'CURRENTLIMITED' state, send SYSTem:DCPS:CLR.

Default

OFF


Last Modified:

5Feb2026

New command for D-series (Fluyt).